2025-05-14 11:11 AM - last edited on 2025-05-16 4:31 AM by Amel NASRI
I have a custom PCB using the STM32F042F. I replaced the STM, and now every time I connect the communication chip, the STM32 turns off. The STM does not boot if I first connect the nRF24L01 then power the STM.
I am confident my code and the board are not the issue, as it was functioning before I replaced the STM32 chip.
I think that some default configuration setting I am missing is causing the boards to short.
Does anyone have any ideas on how I can solve this issue?
2025-05-23 3:40 AM
Hello @JimJones12 and welcome to the community;
I think you have a hardware issue, ensure that the new STM32 is correctly replaced.
Check the power, ground connections and SPI communication lines.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.