2025-10-16 4:51 AM - last edited on 2025-12-29 9:43 AM by ELABI.1
Dear Sir ,
Kindly Help In Writing Program for PFC Boost Control.
As i have worked on making an power supply with Below Specification Details :
Input Voltage : 1 to 20 VAC(Variable)
Input Current : 3Amps (Constant)
We Require :
Output Voltage : 30VDC
Output Current : 3AMPS
For This we already created a closed loop system of power factor correction with boost controller .
in this we take feedback from output using voltage divider .
so i have an request to you kindly any one have solution pls suggest me to do this .
regards,
Nilmani
2025-10-16 5:00 AM
@Andrew Neil Sir Pls Help Me For Doing This .
2025-10-16 6:38 AM
So what have you done so far? Where are you stuck?
you're going to need to give a load more details about your hardware.
See: How to write your question to maximize your chances to find a solution
2025-10-17 12:05 AM
It will be difficult to help you.
However, you can take a look at X-CUBE-DPOWER to see how a PFC is implemented in similar projects. The AN6096 in particular could be a helpful starting point.
Good luck!
Regards
/Peter
2025-10-17 2:27 AM
Dear @Peter BENSCH Sir,
Thank you for your support. I am currently using the STM32F103C6T6 MCU to program a PFC Boost Converter.
This project is quite similar to the reference application you shared AN6096 ; however, the main difference is that I am using the STM32F103C6T6 microcontroller. Therefore, I kindly request your suggestion for any videos, tutorials, or resources that could help me in writing the program.
Additionally, I am using ACS712 (20A) for input current and voltage sensing, and a voltage divider circuit for output voltage sensing.
Input Voltage : 1-20VAC Variable
Input Current:3 Amps Constant
Output Voltage :30 VDC Constant
Output Current :3A Constant
I am Waiting For Your Reference .
Regards,
Nilmani
2025-10-28 10:11 AM
You don't seem to have taken into account any of @Peter BENSCH's points.
@nilmanivas wrote:Input Voltage : 1-20VAC Variable
Input Current:3 Amps Constant
So, at the minimum input voltage (1V), you have only 3W of input power;
at the maximum input voltage (20V), you have 60W of input power.
@nilmanivas wrote:Output Voltage :30 VDC Constant
Output Current :3A Constant
That's 90W of output power, but you have no more than 60W of input - possibly much less!
@nilmanivas wrote:I am using the STM32F103C6T6 microcontroller.
As @Peter BENSCH said, that is likely to be insufficient to the task.
2025-10-30 11:31 PM
Dear @Andrew Neil & @Peter BENSCH Sir,
I am currently working with an input of 30 VAC and 6.5 A, and I would like to achieve an output of 25 VDC With 4 A.
Could you please advise whether this is possible? Additionally, I am aiming for a power factor greater than 0.90, so I would appreciate your guidance on how to achieve this in my setup.
I am Using Stm32f103c8t6 and stm32g031c6t6 microcontroller for Output Voltage Controlling Using Closed Loop System . Here i have input Current Sensor And Output Voltage Sense.
Best regards,
Nilmani
2025-10-31 2:04 AM
@nilmanivas wrote:I am currently working with an input of 30 VAC and 6.5 A, and I would like to achieve an output of 25 VDC With 4 A.
So that's no longer a boost converter - is it?
2025-10-31 2:16 AM - edited 2025-10-31 2:17 AM
pls help me out sir
2025-10-31 2:16 AM
yes sir
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.