2018-10-11 11:00 PM
Hi ,
I am using an STM33L072 with the Keil uVision environment.
I want to prevent a couple of variables from being initialized on startup
The manual says to use
#pragma arm section zidata = "non_initialized"
uint8_t reset_pos;
RtcCalendar_t Current_Time; // Current time is updated from the server when the base station connects
// it is incremented by RTC_AlarmB which is set to 1 minute so ingnore seconds
#pragma arm section zidata // back to default (.bss section)
The map shows them non_initialized
Global Symbols
Symbol Name Value Ov Type Size Object(Section)
reset_pos 0x200036f0 Data 1 mainbase.o(non_initialized)
Current_Time 0x200036f4 Data 28 mainbase.o(non_initialized)
but they are still returning to zero on reset in debug mode
Is there something else I need to do to stop them being set to zero?
Thank You
Regards
2018-10-12 5:03 AM
This is a Keil-specific question, so probably better asked at their forum.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.