2019-04-08 7:18 AM
Hi ,
I’m trying to build a MDK-ARM project with Eclipse (SW4STM32).
I did import the project folder to eclipse : File -> import ->General -> Existing Project Workspace-> My_Project_Folder but the build function doesn’t work !
So I created a new project and I added the sources , in this case, when i make the build , it generates many errors which I didn’t have with Keil .
is there any better way to import a uvision project into eclipse ?
2019-04-08 7:38 AM
"I did import the project folder to eclipse : File -> import ->General -> Existing Project Workspace"
this is for import existing eclipse projects.
In new project you created, check project->properties->C/C++ Code General->Paths and Symbols if all Include paths, #symbols are defined well as in Keil project.
2019-04-08 8:35 AM
Thank you for replying.
The include Paths and symbols are all set and defined, even though I always have "no such file or directory" errors and other problems that appears.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.