2019-03-05 11:21 AM
Hello,
I am programming a SMT32 chip and I am trying to find the size of a defined structure like the code snippet below. From reading online, using sizeof() on a structure can yield different results on different IDEs. When I use sizeof(struct some_struct) in Atollic TrueSTUDIO, I get an error. What do I use to return the size of a structure in Atollic TrueSTUDIO?
struct some_struct{
UINT8 variable1;
UINT8 variable2
UINT32 variable3
};
main(void){
UINT8 strucutre_size;
strucutre_size=sizeof(struct some_struct);
}
2019-03-05 11:58 AM
What errors specifically does it report. Bunch of semi-colons missing if I cut-n-paste
typedef struct _some_struct{
UINT8 variable1;
UINT8 variable2;
UINT32 variable3;
} some_struct;
int main(void)
{
size_t structure_size;
structure_size = sizeof(some_struct);
printf("%d\n", structure_size);
while(1);
}
2019-03-05 12:29 PM
Hello,
You missed some semicolons inside your structure, also the types UINTx may not be defined.
This code must work in True Studio.
struct some_struct{
uint8_t variable1;
uint8_t variable2;
uint32_t variable3;
};
int main(void){
uint8_t structure_size;
structure_size=sizeof(struct some_struct);
}
"some_struct" is 32bit aligned, so after padding the total size reported from sizeof will be 8 bytes.
consider use #pragma pack(x) directive to change the alignment. and/or reorder structure members to reduce the requiring memory or to conform to some specific structure pack format.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.