2019-07-09 3:11 AM
Hello,
I am working with Matlab simulink on a project. After building my blocks model, I want to create a PIL simulation but get some while debugging the code source on True STUDIO as shown in the picture below.
Could you please help with this ?
Thanks
Best regard
2019-08-20 3:17 AM
Hi @IOUMA ,
The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.
While working on this version the followings tests were successful for PIL:
- F429ZITx @ 180 Mhz, USART1: OK
- L476RG @ 80 Mhz, USART2: OK
As far the toolchain is concerned, there are known issues with eclipse-based tools, especially for include paths and build resources that can be defined as excluded.
It is an issue with the project generator that is used.
In the current situation, in the project generated for these types of IDEs, check the include parameters for the paths and verify that the build resource is also enabled.
Sorry for the disturbance.
Regards.
Cyril
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.