2019-07-16 9:07 AM
Hi,
Using Windows 7,
MATLAB R2018b,
STM32-MAT/TARGET 4.4.2
uVision V5.22.0.0
I'M trying the STM32-MAT\STM32\STM32demos\PIL\ADC\TestAdc.slx Simulink Model. The model Build ok in Simulink but when it arrive in uVision it don't link and I have those messages:
linking...
TestPilAdc\TestPilAdc.axf: Error: L6218E: Undefined symbol CA_TestPilAdc_ActHW (referred from coder_assumptions_app.o).
TestPilAdc\TestPilAdc.axf: Error: L6218E: Undefined symbol CA_TestPilAdc_ExpHW (referred from coder_assumptions_app.o).
TestPilAdc\TestPilAdc.axf: Error: L6218E: Undefined symbol CA_TestPilAdc_HWRes (referred from coder_assumptions_app.o).
TestPilAdc\TestPilAdc.axf: Error: L6218E: Undefined symbol CA_TestPilAdc_PWSRes (referred from coder_assumptions_app.o).
TestPilAdc\TestPilAdc.axf: Error: L6218E: Undefined symbol TestPilAdc_caRunTests (referred from coder_assumptions_app.o).
Not enough information to list image symbols.
Finished: 1 information, 0 warning and 5 error messages.
"TestPilAdc\TestPilAdc.axf" - 5 Error(s), 0 Warning(s).
Where can I define those variables?
Regards,
Bruno
2019-08-20 2:25 AM
Hi @BTrem ,
This problem is not reproduced with the version 5.1.0 of STM32-MAT/TARGET, published end of July 2019.
The compilation is ok and execution also with F429ZITx @180Mhz, USART1.
Regards.
Cyril
PS: Build output
*** Using Compiler 'V5.06 update 2 (build 183)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'TestPilAdc'
assembling startup_stm32f429xx.s...
compiling stm32f4xx_hal_msp.c...
compiling main.c...
compiling stm32f4xx_it.c...
compiling stm32f4xx_hal_timebase_tim.c...
compiling stm32f4xx_hal_adc_ex.c...
compiling stm32f4xx_hal_adc.c...
compiling stm32f4xx_hal_tim_ex.c...
compiling stm32f4xx_hal_uart.c...
compiling stm32f4xx_hal_tim.c...
compiling stm32f4xx_hal_rcc.c...
compiling stm32f4xx_hal_rcc_ex.c...
compiling stm32f4xx_hal_flash.c...
compiling stm32f4xx_hal_gpio.c...
compiling stm32f4xx_hal_flash_ex.c...
compiling stm32f4xx_hal_flash_ramfunc.c...
compiling stm32f4xx_hal_pwr.c...
compiling stm32f4xx_hal_dma.c...
compiling stm32f4xx_hal_dma_ex.c...
compiling stm32f4xx_hal_pwr_ex.c...
compiling stm32f4xx_hal_cortex.c...
compiling stm32f4xx_hal.c...
compiling stm32f4xx_hal_exti.c...
compiling TestPilAdc.c...
compiling system_stm32f4xx.c...
compiling const_params.c...
compiling look1_iflf_binlxpw.c...
compiling coder_assumptions_flt.c...
compiling coder_assumptions_hwimpl.c...
compiling TestPilAdc_ca.c...
compiling xil_interface_lib.c...
compiling xil_data_stream.c...
compiling xil_services.c...
compiling xilcomms_rtiostream.c...
compiling xil_rtiostream.c...
compiling rtiostream_utils.c...
compiling coder_assumptions_app.c...
compiling coder_assumptions_data_stream.c...
compiling coder_assumptions_rtiostream.c...
compiling TestPilAdc_ADC.c...
compiling xil_interface.c...
compiling xil_instrumentation.c...
compiling STM32SerialRtiostream-Rtiostream.c...
compiling codeinstr_data_stream.c...
compiling codeinstr_rtiostream.c...
compiling STM32SerialRtiostream-ProfilerTimer.c...
linking...
Program Size: Code=15488 RO-data=33368 RW-data=188 ZI-data=1724
FromELF: creating hex file...
"TestPilAdc\TestPilAdc.axf" - 0 Error(s), 0 Warning(s).
Build Time Elapsed: 00:01:07
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.