2019-04-29 12:15 PM
Dear,
I would like to use STM32G0x0 mcu for my new project, but the eeprom is missing. How to emulate the eeprom from flash? I supose the solution will be different from the STM32Fxx series.. Is not it?
Best Regards, Jan.
2019-04-29 12:26 PM
Honestly, how hard is it to manage a couple of 2KB Flash pages to store the data/structures you need?
2019-04-29 10:46 PM
I do not know, but I have experience with asf lib. from Amel (SAMD21 M0+) and I know there were not so clear steps for saving data to flash... Fro example Lib.c for emulate eeprom has 977 lines of code
2019-04-29 11:21 PM
I rather would be interested in real EEPROM, it only present in L0 series AFAIK. Does anybody know anything about real EEPROM in future chips, or I can forget that?
2019-04-29 11:21 PM
I hope you are aware of the compromises you make with an EEPROM emulation, instead of EEPROM.
2019-04-29 11:42 PM
You would have to ask ST. It is all a matter of sales price vs. use cases. The 16/32 bit wide erase/program capability and the increased durability (erase cycles) come at a price, which a number of large-scale customers is not willing to pay.
Since the EEPROM erase/programming times are in the millisecond range as well, external serial EEPROMs are an option with little timing/code overhead.
2019-04-30 12:09 AM
On the register interface level, the G0's flash controller is (almost) identical to the L4's. It should be fairly straightforward to port x-cube-eeprom and AN4894 to the G0 family.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.