2025-05-08 2:30 AM - last edited on 2025-05-08 2:38 AM by Andrew Neil
HI, I am MURALI SELVAM from India, I need reference design for Below given part number. I want DCMI Camera Interface 8-bit D[7:0](BT.601), PCLK, HSYNC, VSYNC. So anyone who has reference design related that kindly give me.
*****STM32F407VET6
Solved! Go to Solution.
2025-05-08 7:44 AM
Video streaming over USB is feasible as the calculated throughput is within the capabilities of the USB HS interface. Here is an example.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-08 2:44 AM
https://blog.arducam.com/stm32-cameras-that-support-dcmi/
via: https://www.google.com/search?q=8-bit+DCMI+Camera+Reference+Design
and: https://www.st.com/en/microcontrollers-microprocessors/stm32f407ve.html#documentation
2025-05-08 2:56 AM - edited 2025-05-08 2:58 AM
Thanks for sharing that but I need reference schematic like tested board's schematic. If you have kindly share me and Can we do video streaming via USB?
2025-05-08 6:06 AM - edited 2025-05-08 6:21 AM
If it's not what you're looking for, why did you mark it as the solution?
To unmark it, see here.
You can't expect there to be an off-the-shelf design for every possible application just waiting for you; at some point you are going to have to do some actual design work yourself - or pay someone to do it specifically for you...
Why do you particularly want to do this on an STM32F407VET6?
PS:
If you do want an off-the-shelf design, then just go by the performance/feature requirements you need - rather than the processor it runs on.
Sounds like a Raspberry Pi would do ...
2025-05-08 6:55 AM
[Unmarked the solution]
2025-05-08 7:03 AM
Unfortunately, I was clicked Accept as solution.
2025-05-08 7:07 AM
I need reference schematics for the part number for camera interface with CVBS Signal. 8-bit parallel Signal, PClk, VSync with STM32 MCU will give video streaming via USB, is it possible?
2025-05-08 7:44 AM
Video streaming over USB is feasible as the calculated throughput is within the capabilities of the USB HS interface. Here is an example.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.