2009-05-14 2:45 AM
Where are TI1 & TI2?
2011-05-17 6:03 AM
Hi Fangelin,
The user have the possibility to select the ICx(input capture) to be connected into TIM1 Input x(internal connection), you can refer to the: Capture/compare mode register x description (TIM1_CCMRx)in reference manual. Regards mozra2011-05-17 6:03 AM
Target: STM8S207S8
I'd like to use the Encoder interface mode for TMR1, by means of TI1 and TI2: really I can't find the physical access to these signals (are they input pins? if so, where are they located?) Many thanks!2011-05-17 6:03 AM
in STM8S207S8 (lqfp44)
pin24 = pc1/tim1_cc1 = TI1 = TI1FP1 pin25 = pc2/tim1_cc2 = TI2 = TI2FP2 please read 14020.pdf 19.2 tim1 block diagram 19.5.12 encoder interface mode regards2011-05-17 6:03 AM
Many thanks guys!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.