2018-09-19 12:01 PM
TN1235, released this month has some basic information on the new STLINK-V3 (which already can be ordered at some distributors, but lead times are long, and where there are pictures they show the older ST-LINK/V1)
According to TN1235, for the SWIM interface (and thus for using STLINK-V3 with STM8) one needs some adapter board called MB1440. I found no mention of MB1440 outside of TN1235.
When will STLINK-V3 and MB 1440 become available?
Philipp
2018-09-27 6:49 AM
It seems that mouser has 50 on stock:
https://hu.mouser.com/ProductDetail/STMicroelectronics/STLINK-V3SET
2018-09-28 3:56 AM
More information will come mid-october
2018-10-02 1:06 PM
I received a note from someone who bought it at Mouser. Apparently, the STLINK-V3SET comes with the MB1440 included.
Philipp
2018-10-03 1:42 AM
Images and link to USB data on a blog (not mine):
http://users.atw.hu/balubati/blog/index.php?entry=entry181002-114748
Philipp
2018-10-05 5:55 AM
@S C
It is a nice piece of hardware, with excellent capabilities!
Do you know if the protocol for the direct access of the USB-CAN, USB-I2C, USB-SPI will be published?
Documentation to the standard programming capabilities JTAG, SWD, SWIM would be very useful as well. (If not we have to reverse engineer it ;))
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.