2007-05-07 10:11 PM
2011-05-17 12:39 AM
Hi Sunshan
The address is defined on the pins MF0..MF4 at reset. These are read into the PAD register. Eg. If you have an IAR evaluation board (STR912_SK) it is 0x17 If you have the REva_DAUGHTER board it is 0x15. Note: I haven't actually programmed these boards but I have prepared to do it. Therefore it is not 100% guarantied.Regards Mark Butcher www.uTasker.com2011-05-17 12:39 AM
Hi,how can I define the address of the PHY(STE100P)?what is the function of the PAD[4:0]?but there is not the PAD[4:0] pins,the MAC controler is STR912X.
Best Regards sunshan2011-05-17 12:39 AM
Thank you!I will confirm the address of the PHY.There is few information in the STE100P datasheet .
Best regards! sunshan2011-05-17 12:39 AM
Hi mjbcswitzerland.In the code of Ethernet Library,the function Ethernet_Init() define the address of PHY is 0x00.but the data which I read from PR20-XMC is 0xaa(PAD4:0 10101).when I think the address of the PHY is 0x00,I also can read ID of PHY(STE100P)and the ID is right.So what I wonder is that what is the address of PHY ,how to define ?In my evaluation board the Mf4:0 is 10111.I appreciate your help.
Best Regards sunshan2011-05-17 12:39 AM
Hi sunshan
I have just started working with teh PHY and have also found that it responds to address 0x00. I have started a new thread about the subject. If I can find any more details I will follow up there. Regards Mark2011-05-17 12:39 AM
hi mjbcswitzerland
The address is defined on the pins PAD[4:0].but I found that the address of PHY is 0x00 or the PAD[4:0].both of them is right.I don't understand why.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.