cancel
Showing results for 
Search instead for 
Did you mean: 

Silicon Bug or mistake in Datasheet? on ETM_EXTRIG MII_MDC port 1.7

mark9
Associate II
Posted on March 16, 2007 at 03:22

Silicon Bug or mistake in Datasheet? on ETM_EXTRIG MII_MDC port 1.7

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
mark9
Associate II
Posted on May 17, 2011 at 09:39

Port 1.7, aka ETM_EXTRIG or MII_MDC causes weird behavior if SCU_GPIOIN1.7 is not 1. Supposedly, if this bit is cleared, then nothing happens on this pin according to table 4 of the data sheet. However, if the MII is used, whenever a packet arrives, the debugger halts!

I looked at the documentation, and it seems there is a feature on Port 3.0 that has a similar feature. cf EXT_ETMT_EDBGR and P30_SELEDBG on SCU_SCR0. But Port 3.0 is not Port 1.7.

Is there a mistake in the datasheet, table 4? Is the default input behavior of Port 1.7 actual ''External Debug Request''? Or is this a silicon bug?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.