2008-04-09 1:06 AM
2011-05-17 12:51 AM
The Watchdog seems to behave a bit strange.
I trigger the Watchdog in a while-loop like: while(timerExpired == false) { TrigWD(); } TrigWD() { WDG->KR = 0xA55A; WDG->KR = 0x5AA5; } In this case the cpu will sometimes crash, even though WD is triggered all the time. If I change the code to: TrigWD() { WDG_Cmd(ENABLE); } The cpu will also crash I tried to change the code to not trigger the watchdog all the time: TrigWD() { if(WDG->CNT < 0x76) // preload value is 83 { WDG->KR = 0xA55A; WDG->KR = 0x5AA5; } } It still crashes.... But if I change the function to TrigWD() { if(WDG->CNT < 0x76) { WDG_Cmd(ENABLE); } } It will work fine. Is there a problem when triggering the WatchDog to often? Have anyone seen this? Is it a silicon limitation? I am running the cpu at 94,5 MHz and using RTC clock for WD. The compiler is GCC.2011-05-17 12:51 AM
Try (as an experiment) to run the watchdog from the PCLK instead of RTC. I had a similar problem with the watchdog on RTC. The problem was that if there was a WD reset, the WD would continue to be enabled *after* the reset, so it would immediately have another WD reset. This was extremely repeatable.
Mark2011-05-17 12:51 AM
Hello rickard.thorstensson, lakata,
This problem is never seen before. I tried to use the WDG reset with the RTC as clock source and fCPU=96MHz. However, I didn't see any crash. Could you please send me a simple code where you can reproduce this problem. Thank you in advance and best regards, mirou. [ This message was edited by: mirou on 08-04-2008 10:22 ]2011-05-17 12:51 AM
[This post handled another problem, removed]
[ This message was edited by: rickard.thorstensson on 09-04-2008 13:59 ]2011-05-17 12:51 AM
Ignore my previous post, it was another problem. The real problem seems to be that the compiler don't store the registers r0,r1,r2,r3 in functions before modifying them, causing a instable behaviour. The code worked when I changed the timing since no damage was caused by the register change.
I.e. the compiler should do like this void Function() { stmdb sp!, {r0,r1,r2,r3, lr} mov r0, #256 ; 0x100 mov r1, #1 ; 0x1 ... if r0 to r3 are used in the function. but it doesn't do that, it do like this: void Function() { mov r0, #256 ; 0x100 mov r1, #1 ; 0x1 Is there any configuration to tell the compiler to store r0 to r3 also? Why does the compiler behave like this? Is it a bug? I'm using GnuArm 4.1[ This message was edited by: rickard.thorstensson on 09-04-2008 13:58 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.