2016-08-16 9:44 AM
How i calculation junction temperature in VIPER37HD/LD
and how the frequency(60k,115k hz) Affect on junction temperature?2016-08-18 5:56 AM
Hello,
The junction temperature is given by the following formula:
Tj = Pdiss • Rth_ja + Ta
where:
Ta = ambient temperature
Rth_ja = junction-to-ambient thermal resistance (reported on datasheet, its value can be reduced providing adequate copper area around DRAIN pins) </p>
Pdiss = Pbias + Pcond + Pswitch + PCAP is the power dissipated within the VIPer, in particular:
Pbias = VDD • IDD1 (bias losses)
where:
VDD = voltage of the VDD pin (depends on the voltage delivered by the auxiliary winding of the transformer);
IDD1 = VIPer consumption, in switching conditions (reported on datasheet)
Pcond = Rdson • Irmsp conduction losses
where:
Rdson = on resistance of the VIPer (reported on datasheet)
Irmsp = primary RMS current (depends on input/output conditions, primary inductance, reflected voltage)
</p>
Pswitch = (Vin + VR) • Ipk • Tc • fsw/3 switching losses is an approximate formula where
where:
Vin = input voltage
VR = reflected voltage
Tc = crossover time (the time during which, at turn-off, both DRAIN voltage and current are not zero), should be estimated and is in the range of some tens nsec
fsw = switching frequency
Ipk = primary peak currentPCAP = Cdrain_par • Vds2 • fsw/2
where:
Cdrain_par = sum of all the capacitance of the DRAIN node (MOSFET output cap, reported on datasheet, plus stray capacitances due to the transformer)
Vds = DRAIN voltage value at turn-on
The components PCAP and Pswitch depends linearly on the switching frequency
From: biton.pini
</span>
</span>
</span>
Posted: Tuesday, August 16, 2016 6:44 PMSubject: viper37 junction temperatureHow i calculation junction temperature in VIPER37HD/LD
and how the frequency(60k,115k hz) Affect on junction temperature?2016-08-19 12:06 AM
thanks alot for your help
Pcond = Rdson • Irmsp conduction losses
you meant that the current in Square ?and if you explain more what exactly Tcbest regardpinhas2016-08-22 1:12 AM
-Iprms
is the root mean square of the primary current
-Tc
At the end of the MOSFETs ON time, the DRAIN current has reached its maximum, while the DRAIN voltage is zero, thus the product IDRAIN*VDRAIN = 0W
Some time after turn on, IDRAIN will be 0 and VDRAIN will be Vin + VR, so again IDRAIN*VDRAIN = 0.
But in between, since the switch is not ideal, there is a time interval Tc when both IDRAIN and VDRAIN are >0, and so their product results in power dissipation at turn off.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.