cancel
Showing results for 
Search instead for 
Did you mean: 

ST1CC40DR too hot on 3A

pavel2
Associate
Posted on August 08, 2016 at 21:51

Hi! I have made a scheme for CREE X-ML2 LED (with maximum output at 3A) in eDesign studio. But missed that IC loses 0.8w power at 3A and getting very hot quickly, then stepdown output current to ~2A. Is there any way to fix it without total redesign(with different IC) or big additional heatsink on IC?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Patrizia BELLITTO
ST Employee
Posted on August 24, 2016 at 12:10

Dear sir,

the ST1CC40 is a synchronous step down current source with internal high side and low side switch. The switching frequency is fixed and equal to 850KHz. For these reasons, the power losses of the device are due to the selected application conditions, not to the external components selection. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.