2003-10-13 1:57 AM
2011-05-17 2:55 AM
Hey,
I have Serial Port 0 working fine (receiving and transmitting), but now I want to use an interrupt triggered routing for receiving data. I can't get the program to run the correct ISR to clear the RI bit. Here's my code to set up the interrupt: PS = 1; /* set high priority for USART */ ES = 1; /* enable USART 0 interrupt */ EA = 1; /* enable interrupts */ Here's my code for the ISR routine: static void USART_isr (void) interrupt SIO_VECTOR using 2 { unsigned char temp; if (RI) //If Receive buffer is full { temp = (SBUF); //Retrieve Buffer RI = 0; //set RI bit to 0 } } very simple code, but can't seem to get it go to the ISR. Any suggestions, comments?? Thanks, Mike2011-05-17 2:55 AM
Thanks, for the reply
Interrupt initialization: void Interrupt_init (void) { EA = 0; /* disable interrupts */ timer0_tick = 0; TR0 = 0; /* stop timer 0 */ TMOD &= 0xF0; /* clear timer 0 mode bits - bottom 4 bits */ TMOD |= 0x01; /* put timer 0 into 16-bit no prescale */ // Calculate timer tollover based on FREQ_OSC to be 10ms periods timer0_value = 0x10000 - ( ((FREQ_OSC * 5L) / 6L) - 17L); TL0 = (timer0_value & 0x00FF); TH0 = (timer0_value >> ; PT0 = 1; /* set high priority for timer 0 */ ET0 = 1; /* enable timer 0 interrupt */ TR0 = 1; /* start timer 0 */ PS = 1; /* set high priority for USART */ ES = 1; /* enable USART 0 interrupt */ EA = 1; /* enable interrupts */ } No interrup is being generated on transmit. I only want an interrupt to be generated on receive. void Serial_Transmit(unsigned char value) { unsigned int clock_buf; //Disable Interrupts EA = 0; //Enable RTS signal P4_3 = TRUE; SBUF = value; // Xmit the Char while (TI == 0); // Wait Loop till finished xmit of last char TI = 0; //set TI bit to 0 //extend the RTS signal to include the stop bit for (clock_buf=0; clock_buf { clock_buf++; } //Disable RTS signal P4_3 = FALSE; //Enable Interrupts EA = 1; }2011-05-17 2:55 AM
Oh, sorry,
SCON is set to 0x50 Serial receive and trasmit works perfect, if I disable the interrupts. Timer 2 is used for baud rate generation, buad rate is perfect at 19200. Timer 0 is used for something else, and also calls interrupts. I'm having a hard time with this one. If I manually clear the RI bit, I'm fine, but I need it to generate an interrupt on receive and go to the ISR so I can clear the RI bit that way.2011-05-17 2:55 AM
Viper21,
This is a crazy idea, but I don't see anything wrong with your code. The only thing I don't see is the #define for SIO_VECTOR. If you're using Keil C and the first USART, this should be defined as 4. Otherwise, you might be setting up an ISR for the other USART. Best Regards, PhazeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.