cancel
Showing results for 
Search instead for 
Did you mean: 

USART doesn't work at STM8A5188T, Help please !

zsu
Associate II
Posted on September 10, 2009 at 21:37

USART doesn't work at STM8A5188T, Help please !

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
zsu
Associate II
Posted on May 17, 2011 at 15:04

I'm using USART in STM8A5188T (48pin package) at 16MHZ. Timer and ADC works well. But USART does not work at all. No any USART special register could been updated (modified) even during debugging. instructions as below. Any help will be appreciated.

(BTW, LINUART in STM8A5188T works fine.)

USART_BRR2 = 0x02 ;

USART_BRR1 = 0x68 ; // Baud rate at 9600.

USART_CR1 = 0x00 ;

USART_CR3 = 0x00 ;

USART_CR4 = 0x00 ;

USART_CR5 = 0x00 ;

USART_CR2 = 0x2c ;

:-Y

zsu
Associate II
Posted on May 17, 2011 at 15:04

:p

Solved. Clock to USART was turned off.

Hope it help you to avoid same mistake.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.