2009-09-11 1:24 AM
STM8S103F3 tsspop20 Alternate Function Remapping AFR0
2011-05-17 6:04 AM
Hi,
I'm having trouble trying to remap TIM1_CH1 and TIM1_CH2 using AFR0 option bit. In the memory window in debug mode, Option Byte @0x4803 holds de right value, but I can't get the output to change state on the proper pins. I have TIM1_CH3 and TIM1_CH4 working just fine with the exact same configuration as _CH1 and _CH2. So I know this is not a configuration issue. Is there any specific algo to follow at power-up to make sure alternate function remapping works or is there any issue with that particular remapping on that device? Thanks, Francis Savaria2011-05-17 6:04 AM
Hi,
Did you read value @0x4804? It'd equal to FEh, if not try to write 01h @0x4803 and FEh @0x4804 and then reset the device. coluber2011-05-17 6:04 AM
Alright, here is some information I forgot to tell:
- I work with Raisonnace Ride7 environment; - Option bytes OPT2/NOPT2 values were validated through Memory View debug window and through Option debug window; - Current desired remapping is 0x05/0xFA (AFR0 & AFR2), but TIM1 OC1 and OC2 still won't work, while OC3 and OC4 are alright; - I tried AFR0 both alone and with AFR2. I have designed an alternative for what I need to accomplish, but the day I'm going to need those outputs working is not far. Did I hit a bug or am I just clueless? :-] Merci d'avance, Francis Savaria2011-05-17 6:04 AM
Hi,
I've tried your configuration, previously setting both AFR0 and AFR2 and I can see correctly toggle TIM1_CH1(PC6) and TIM1_CH2(PC7). coluber2011-05-17 6:04 AM
So I must be clueless... :-[
[...] // set alternate function remapping FLASH_ProgramOptionByte(0x4803, (AFR0|AFR2)); [...] // init outputs GPIO_Init(GPIOC, (GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_4 | GPIO_PIN_3), GPIO_MODE_OUT_PP_LOW_SLOW); [...] // enable OC outputs TIM1->CCER1 |= (u8)(TIM1_CCER1_CC2E | TIM1_CCER1_CC1E); TIM1->CCER2 |= (u8)(TIM1_CCER2_CC4E | TIM1_CCER2_CC3E); [...] All values in the control and config registers are what I want them to be (all 4 channels with the same config) and OC1 (TIM1_IER_CC1IE) interrupt is even working! PC7 and PC6 are working fine as GPIOs. So... what else do you think I should look for?2011-05-17 6:04 AM
Hi,
In my example I set CCMR1,CCMR2,CCMR3,CCMR4 to 60h (PWM mode1), also MOE is set, and no need to initialize PORTC. I hope this can help you. coluberWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.