cancel
Showing results for 
Search instead for 
Did you mean: 

UART2 interupt problem

jones2
Associate II
Posted on February 18, 2004 at 14:44

UART2 interupt problem

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jones2
Associate II
Posted on May 17, 2011 at 11:58

Hello,

I have trouble getting uart 0 and 1 interrupts, I will

try to set high priority, but even so, I have an error that

I don't understand, and I suspect it might be the problem.

In the ''upsd3200.h'' appears:

// --- UART2 SFRS ----

sfr SCON2 = 0x9A; // UART2 Serial Control

sfr SBUF2 = 0x9B; // UART2 Serial Buffer

and:

/* SCON 2 */

sbit SM02 = SCON2^7;

sbit SM12 = SCON2^6;

sbit SM22 = SCON2^5;

sbit REN2 = SCON2^4;

sbit TB82 = SCON2^3;

sbit RB82 = SCON2^2;

sbit TI2 = SCON2^1;

sbit RI2 = SCON2^0;

I get errors regarding the sbit declarations:

..\COMMON\UPSD3200.H(474): error C146: 'SCON2': invalid base address

what could it be?

jdaniel
Associate II
Posted on May 17, 2011 at 11:58

steadicopter,

SCON2 is not a bit-addressable SFR, only SCON is. As such, Keil won't let you define SFR bit variables (sbit) for this register. You'll have to use masks to turn individual bits on and off. As a matter of fact, I don't know how you could have a problem other than this error, because this will prevent you from compiling your source. Hope that helps.

Best Regards,

pHaze426
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.