2004-02-18 3:17 AM
2011-05-17 2:58 AM
sjo,
Thanks for the suggestion. I think that would probably solve my problem, however that still leaves me having to connect and disconnect the plug for the reset line every time I want to program. I've also hacked around a bit more and found that as long as I do some JTAG operation with PSDSoft after a reboot and before I start the emulator, things seem to work ok. Will the mysteries of Windows never cease? Regards, pHaze4262011-05-17 2:58 AM
I have a question concerning the use of ST's Flashlink programmer in Windows 2000. Generally, everything seems to work correctly for me with PSDSoft Express and the JTAG port on my target, however, I have some problems at Windows startup that I wonder if ST has a solution to.
If I have my target running and have the flashlink cable plugged in (as I tend to leave it for code, compile, program, debug cycles) and I restart my computer, it seems to place the target in reset and halt program execution. This normally isn't a problem, but I just purchased a Nohau emulator system which requires the Flashlink cable to program a PSD device after code changes. If the Flashlink cable is left plugged in, however, it seems to prevent the emulator from functioning. I spoke to Nohau support and it seems to be operating system specific as they couldn't reproduce the problem on Win98SE. Basically, I wonder if there is some utility I could run to place the parallel port and flashlink box into a known good state so that my emulator will still function after I download code. If I have to keep plugging in and unplugging the cable, the whole emulator setup will certainly lose some of its efficiencies. Any help would be greatly appreciated. Best Regards, pHaze4262011-05-17 2:58 AM
As a thought have you tried using the other cable (10way to loose terminals) given with Flashlink, and connect all the pins except the reset. Flashlink resets the device after a program, but with this removed the emulator would have control.
May help your problem. Regards sjo2011-05-17 2:58 AM
Glad you have solved your problem.
Back to my above idea, you would not have to keep removing the reset - just leave it disconnected. You do not have to reset the uPSD to progam it - JTAG does not even require a reset pin to work. Have a look at the jtag application note. The emulator would perform the reset after the programming operation. Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.