2008-09-19 1:43 AM
2011-05-17 12:55 AM
Hi
My UART0 is sending very well, but it cant receive nothing! :| Can anyone give a tip please? Thanks :o here is the code: UART_InitTypeDef st_UART0; GPIO_InitTypeDef GPIO_InitStructure, GPIO_InitStructure2; /* Enable the GPIO3 Clock */ SCU_APBPeriphClockConfig( __GPIO3, ENABLE ); SCU_APBPeriphReset(__GPIO3, DISABLE); SCU_APBPeriphClockConfig( __GPIO5, ENABLE ); SCU_APBPeriphReset(__GPIO5, DISABLE); SCU_APBPeriphClockConfig(__UART0, ENABLE); SCU_APBPeriphReset(__UART0, DISABLE); /* Configure UART1_Rx pin GPIO5.1 */ GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; //GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1; GPIO_Init( GPIO5, &GPIO_InitStructure); /* Configure UART1_Tx pin GPIO3.4 */ GPIO_InitStructure2.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure2.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure2.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure2.GPIO_IPConnected = GPIO_IPConnected_Enable; GPIO_InitStructure2.GPIO_Alternate = GPIO_OutputAlt3; GPIO_Init( GPIO3, &GPIO_InitStructure2 ); UART_DeInit(UART0); st_UART0.UART_WordLength = UART_WordLength_8D; st_UART0.UART_StopBits = UART_StopBits_1; st_UART0.UART_Parity = UART_Parity_Odd ; st_UART0.UART_BaudRate =115200; st_UART0.UART_HardwareFlowControl = UART_HardwareFlowControl_None; st_UART0.UART_Mode = UART_Mode_Tx_Rx; st_UART0.UART_FIFO = UART_FIFO_Disable; // st_UART0.UART_TxFIFOLevel = UART_FIFOLevel_1_2; //st_UART0.UART_RxFIFOLevel = UART_FIFOLevel_1_2; UART0->ICR = 0x3ff; // CLEAR_ALL_INTERRUPTS UART_ITConfig(UART0, 0x10, ENABLE);/// just RXIM its 0x10 UART_LoopBackConfig(UART0, DISABLE); UART_IrDACmd(IrDA0, DISABLE); UART_Init(UART0, &st_UART0); UART_Cmd(UART0, ENABLE); VIC_Config(UART0_ITLine, VIC_IRQ, 10); VIC_ITCmd(UART0_ITLine, ENABLE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.