2007-03-05 2:28 AM
UART RX DMA - The Right way to work ?
2011-05-17 12:36 AM
hi,
I have downloaded one of the examples from this site (UART_Interface-DMA.zip) that implements UART RX DMA, the sample works good The len of my data packets is not fixed, it can be 12 bytes to 80 bytes, In this sample, The dma interrupt accures when all the requested data arrives (16 bytes), so a message of len 12 bytes can wait in the buffer until another message will arrive and trigger the interrupt. What is the right way to do this ? Is it possible to define timeout on the dma, so I will get interrupt when part of the data arrives and timeout had past from the last byte received ? Thanks2011-05-17 12:36 AM
Hi,
I am in the same situation. The interrupt is generated only when the UART fifo is reached. Here is my setup : UART_RX fifo level: 8 bytes flow control: peripheral I start the DMA transfert (8 bytes) in the UART interrupt. If the message is more than 8 bytes, the first bytes are missing ?? I still searching ...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.