Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Starting Stm8s GPS speed device

Posted on May 15, 2011 at 19:19Hello, At the beginning, I must say that I am a beginner in microcontrolers... I have to project GPS speedometer device based on stm8s discovery, LCD(nokia 3310), GPS module and some kayboard, I have all the parts, but...

pietruha8 by Associate II
  • 1928 Views
  • 3 replies
  • 0 kudos

UART2 Interrupt

Posted on June 24, 2010 at 10:36Hello i'm port uart2 polling receive data from hyperterminal it's ok. but i need use uart2 receive data with interrupt?   TIM3_DeInit();     TIM3_TimeBaseInit(TIM3_PRESCALER_1,0xFFFF);    TIM3_ITConfig(TIM3_IT_UPDATE...

uthenb by Associate II
  • 1139 Views
  • 3 replies
  • 0 kudos

Testing timer overflow flag in ISR

Posted on May 11, 2011 at 10:31Hi, I am using STR7 microcontroller and I have problems with checking the state of Timer3, in ISR triggered by Timer2. Timer3 works in PWM mode and produces 125kHz waveform. It is not configured to generate interrupts...

ptrela2 by Associate
  • 1648 Views
  • 1 replies
  • 0 kudos

From AVR (AVR-GCC) to STM8 with STM8S-Discovery

Posted on May 05, 2011 at 16:31Good day! I'm writing my first project with STM8. Here are a couple of questions: - AVR-GCC has a convenient attribute PROGMEM (http://www.nongnu.org/avr-libc/user-manual/pgmspace.html) to store data (for example big a...

artvolk by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.