2003-03-24 12:40 AM
the problem about writing xflash in 72f264
2003-03-18 2:42 PM
hello, I meet a problem that I use indart 72f264 demo board to write
some context in 264. firstly , I want to unlock the rass with writing FCSR #$56,#$ae, but it seems that I didn't success because I can not set the fcsr,#1. The indart soft give me a communication error message when I step by step to implement the instruction ''BSET FCSR,#1'' after implement .main LD a,#$56 LD FCSR,A LD A,#$AE LD FCSR,A how can I do ? thx![ This message was edited by: PIKKABALL on 19-03-2003 04:13 ]2003-03-23 6:59 PM
Hello,
I hope you know that once the LAT bit in FCSR is set, you cannot execute anything from flash. Hence it is necessary to jump to RAM before setting LAT bit. This could be the cause of the communication error.2003-03-24 12:40 AM
AN1477 (Emulated Data EEPROM with XFlash memory) available in this site (download part) gives you all the code to do that! Moreover, the example is made with a 264!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.