2019-12-19 4:08 AM
I2C_Cmd(sEE_I2C, ENABLE);
/* sEE_I2C configuration after enabling it */
I2C_Init(sEE_I2C, I2C_SPEED, I2C_SLAVE_ADDRESS7, I2C_Mode_I2C, I2C_DutyCycle_2,
I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);do the init order have some problem?
below one is common:
void Init(void)
{
I2C_DeInit(I2C1);
I2C_Init(I2C1,IICSPEED, host_address, I2C_Mode_I2C,I2C_DutyCycle_2, I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);
I2C_Cmd(I2C1,ENABLE);
}I2C_Cmd(sEE_I2C, ENABLE);
I2C_DeInit(sEE_I2C);
/* sEE_I2C configuration after enabling it */
I2C_Init(sEE_I2C, I2C_SPEED, I2C_SLAVE_ADDRESS7, I2C_Mode_I2C, I2C_DutyCycle_2,
I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);is there some bug like above
Solved! Go to Solution.
2019-12-19 7:56 AM
I think I'd have the Cmd before the DeInit.
For ST's I2C the usual means to set up is Cmd then Init, issue with the pins and I2C peripheral getting stuck in BUSY state.
2019-12-19 7:56 AM
I think I'd have the Cmd before the DeInit.
For ST's I2C the usual means to set up is Cmd then Init, issue with the pins and I2C peripheral getting stuck in BUSY state.
2019-12-19 7:08 PM
issue with the pins and I2C peripheral getting stuck in BUSY state?
could you say more about it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.