2019-12-26 2:57 AM
we are putting the
Controller in halt mode after configuring a external interrupt to wakeup. We read in datasheet, halt mode current is 440na. But we are getting current in terms of ( 1ma - 2 ma). Sometimes getting 200ua. It keeps varying. We want halt mode current to be less than 70ua.
STEPs followed below calling halt()
* Switch clock from HSI to LSI Low frequency
* Clear external interrupt flags EXTI->SR1 = 0x00; EXTI->SR2 =
0x00;
* Switch off all peripherals CLK->PCKENR1 = 0x00;
CLK->PCKENR2 = 0x00; CLK->PCKENR3 = 0x00;
* Configuring FLASH register also . (PWR->CSR2 = 0x02;)
* Halt().
Kindly advise.
2019-12-26 3:26 AM
Set pwm and check proper switch hsi to lsi.
Then dont turn off peripherial clock, set peripheria to that state that the board wont draw external cussent (example setting pin high will draw less current than setting pin low with led reverse biased towards pin).
Check amps.
Debugging that kind of thing can be hard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.