2004-12-17 1:22 AM
Systemclock programming (PRCCU-Block) problems
2004-12-15 9:49 PM
Hi,
We are using in our project the STR710FZ2T6-Processor and have the following big Problem: We need to program the PRCCU-block to obtain the outputfrequency RCLK of 28MHz (with a input at CK of 4MHz) therefore we program the PLL1-Registers with the following Data: PRCCU_PLL1CR=0x00000063 -> MX0=0/MX1=1(PLL mult. x 28), FREF_RANGE=1,DX2..0=011 PRCCU_CFR=0x00000009 -> DIV2=0, CK2_16=1, CSU_CKSEL=1; With these port settings we expect a outputfrequency of 28MHz but obtain only 24MHz via the CKOUT-Pin of the CPU! We checked out all ohter configurations of the MX-Bits. The outputfrequencies of the other MX-combinations are connect (12/16/20Mhz). What's going wrong? Is it not possible to get the right Frequency on a multiple factor of 28 (MX1=1, MX0=0) ? Are there any workarounds or is the Chip not able to generate a Frequency with a multiple factor of 28 for the PLL1 ? regards, CEL-TeamWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.