2007-06-26 4:14 AM
Switching between flash BANK 0 and BANK 1 on STR9 (Rowley CrossWorks)
2011-05-17 12:44 AM
hi,
has anybody tried to switch between flash bank 0 and bank 1 on str9 using jtag and rowley crossworks 1.7 environment? i can only change the value of csx bit from 0 to 1 but i can't change it back to 0. i make use of J A V A S C R I P T console and the scripts supplied with the package for str9 by rowley. i call iscprogramconfiguration(0,0,1,0,0,0) function to set csx bit to 1 (bank 1) and iscprogramconfiguration(0,0,0,0,0,0) function to set csx bit to 0 (bank 0). the function doesn't complain about 0 parameter as csx so i assume that it is allowed. there is actually the way to go back to csx = 0 but only by clearing nonvolatile configuration memory. should i expect the iscprogramconfiguration() function to work in the way i use it? or maybe clearing the nonvolatile configuration register is the only way?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.