2007-07-02 12:33 AM
Uart reception by IT and emission by DMA
2011-05-17 12:44 AM
Hello,
I am trying to do the following: To have an interruption each time I received a byte on the UART. To emit a buffer of data by DMA transfer. The problem I have is that if I want an interruption each time I received a byte I have to disable the UART FIFO (because even in 1/8 fifo event, I have an interruption only every 2 bytes). And if I disable Fifo, DMA don't work... I also tried to disable fifo when I am waiting for incomming bytes and enable it when I emit data. But the DMA interruption occured before the FIFO is empty, so if I immediatly disable Fifo I lost the last 4 bytes and If i wait for the fifo to be empty I am wasting 1500µs. Do you have any suggestion?2011-05-17 12:44 AM
I have the same problem with my application, and I also don't know how to solve it. If there just where a TX-complete interrupt, based on the ''Busy'' bit in flag register of the uart it would solve the problem.
If I find a solution how to generate an interrupt at the end of transmission I will let you know...2011-05-17 12:44 AM
Hi again
I have solved my problem by using ReceiveTimeoutInterrupt. I simply wired my Tx to the Rx, though I loose my full duplex it works in my application. Now I have Interrupts when I receive, and when the TxFIFO i empty.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.