2008-09-22 5:47 PM
2011-05-17 12:55 AM
Hi all ,
For S/W delay i just wrote For loop of Multiple of (96000 * 10000) But It gives delay in just microseconds.I am using Ride Simulator. PLL is 96Mhz. Also if anybody has Timer Interrupt Configured for 1ms please send me. Because i am not getting exact delay observed on CRO. Please Reply Regards Sai2011-05-17 12:55 AM
The timer reset behavior is not intuitive. See this post for details:
http://www.st.com/mcu/forums-cat-7126-21.html Matt2011-05-17 12:55 AM
Thanks Matt
What about S/w delay. Regards Sai2011-05-17 12:55 AM
Sorry, I'm confused about your question.
When you say S/W delay, do you mean a simple loop or do you mean configuring the timer to interrupt at a given delay? If you mean a loop, what exactly is your question? And if you mean a timer interrupt, please post your code, expected behavior, and observed behavior so the forum can have a better idea what your problem is. Matt2011-05-17 12:55 AM
Hi all,
By s/w delay I mean to say simple for loop. Clock configuration done is as follows: /*wait state insertion: This function should be executed from SRAM when*/ /*booting from bank1 to avoid Read-While-Write from the same Bank.*/ FMI_Config (FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0,FMI_PWD_ENABLE, FMI_LVD_ENABLE, FMI_FREQ_HIGH);/*Insert 2 Wait States for read*/ SCU_PLLFactorsConfig (192, 25, 2); /* PLL factors Configuration based on*/ /* a OSC/Crystal value = 25 MHz*/ SCU_PLLCmd (ENABLE); /* PLL Enable and wait for Locking*/ SCU_RCLKDivisorConfig (SCU_RCLK_Div1); /* RCLK @96Mhz */ SCU_HCLKDivisorConfig (SCU_HCLK_Div1); /* AHB @96Mhz */ SCU_FMICLKDivisorConfig (SCU_FMICLK_Div1);/* FMI @96Mhz */ SCU_PCLKDivisorConfig (SCU_PCLK_Div2); /* APB @48Mhz */ SCU_MCLKSourceConfig (SCU_MCLK_PLL); /* MCLK @96Mhz */ Delay Function: // ms delay void Delay(unsigned int uint_TimeDelay) { unsigned int l_uintdelay1, l_uintdelay2; for (l_uintdelay2 = 0; l_uintdelay2 < uint_TimeDelay; l_uintdelay2++) { //approx: 96000 instruction execution time (at 96 MHz MCLK) = 1ms minimum for (l_uintdelay1 = 0;l_uintdelay1 for (l_uintdelay1 = 0;l_uintdelay1 } } Delay used in application: while(1) { GPIO_WriteBit(GPIO9,GPIO_Pin_3,Bit_RESET); Delay(1); GPIO_WriteBit(GPIO9,GPIO_Pin_3,Bit_SET); Delay(1); } Expected Waveform (GPIO9.3): OFF time: 1 ms min ON time: 1 ms min Waveform observed on Oscilloscope (GPIO9.3): OFF time: 1 us ON time: 1.36 us I am using RIDE7 debugger.Crystal used is of 25MHz.So delay should be more than the expected but how it can be less than the expected? Regards Sai2011-05-17 12:55 AM
Define your variables in your delay loop as volatile - that way the compiler wont optimize them out. If you are getting 1us times, then most likely that is whats happening.
2011-05-17 12:55 AM
Thanks for Reply
Now I am using timer for delay. But i will definitly use for loop with ''nop'' for small time delay Regards Sai2011-05-17 12:55 AM
Hi,
I had this problem : How to realise a delay.. and in fact, he doesn't work with a simple ''for'' loop : Compiler optimization, i think detect your ''for'' loop empty, and jump directly to the following line of code (TBC).Can i suggest you to add this line just in your loop for :
and will solve (i think) your problem
should be :
for (i=0;i
{
asm volatile ( ''NOP'' );
}
But keep in mind, it's a lot of CPU cycle lost here... A timer is really better especialy for a long periode like 1msec Regards Damien [ This message was edited by: dhoyen on 12-09-2008 10:32 ] [ This message was edited by: dhoyen on 12-09-2008 10:34 ]
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.