2005-07-04 9:43 PM
2004-06-24 1:00 AM
Hi,
I'm working with STVD7 3.0 (Cosmic Toolchain) and target MCU ST7FLITE29. I want to use the onboard data eeprom. I know that the eeprom area must be defined in the linker command file but I cant find the way to do it in STVD7. Of course I can do it manually by simply add ''+seg .eeprom -b 0x1000 -m256'' in the .lkf file, but I want STVD7 to do it. All other segments can be defined in the Linker->Input options, but not eeprom. Why? Regards bood2004-07-01 9:10 PM
Apparently there was not enough room on the window for displaying all the possible options and the EEPROM was not implemented. You just have to untick tha auto check box and add the correct lines in the .lkf file which I guess you already did.
Do you feel that this is a real draw-back ?[ This message was edited by: Alaini on 02-07-2004 09:41 ]2004-07-01 10:01 PM
Thanks for response.
I believe that data eeprom is commonly used in applications. Therefore it's a pity that the Auto function cant be used in such cases because of lacking window space !? Regards bood2004-07-06 9:40 PM
Hi Bood,
thats's what I told to the development team. They are thinking how to overcome this limitation but the solution is apparently not so simple. Sorry for the inconvenience.2005-06-28 2:21 PM
Hi All,
a simple trick to solve the problem: add the following lines to the ''Pre-Link'' tab of Project Settings: cmd.exe /C rename $(OutputPath)$(TargetSName).lkf $(TargetSName).$$$ cmd.exe /C echo # > $(OutputPath)$(TargetSName).lkf cmd.exe /C echo # >> $(OutputPath)$(TargetSName).lkf cmd.exe /C echo +seg .eeprom -b 0x1000 -m256 >> $(OutputPath)$(TargetSName).lkf cmd.exe /C echo # >> $(OutputPath)$(TargetSName).lkf cmd.exe /C echo # >> $(OutputPath)$(TargetSName).lkf cmd.exe /C copy $(OutputPath)$(TargetSName).lkf+$(OutputPath)$(TargetSName).$$$ $(OutputPath)$(TargetSName).lkf cmd.exe /C del $(OutputPath)$(TargetSName).$$$ the result is that the LKF file contains the eeprom seg definition Regards StefanoM2005-07-04 9:43 PM
Very clever Stefano but take care that you make the assumption that the lkf file is regenerated each time by STVD7. This may not be true in the next version so check that the trick works with each new version of STVD7.
[ This message was edited by: Alaini on 06-07-2005 09:55 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.