2011-11-15 8:48 PM
I just received my stm8s-discovery and I'm trying to follow this:
http://benryves.com/journal/3567231
I keep on getting the following error even though I see this function defined in stm8s_conf.h:#error clnk Debug\project.lkf:1 symbol _assert_failed not defined (Debug\stm8s_gpio.o )
I'm clueless on why _assert_failed() isn't being defined in the object file... EDIT: If I don't #include ''stm8s.h'' it compiles just fine.2011-11-22 8:48 PM
Edit stm8s_conf.h to comment out #define USE_FULL_ASSERT (1)
which is about 23 lines from the bottom. I had a same or similar problem with STVD and solved it with the above. I had since then use IAR.2013-11-11 9:18 AM
Hello,
I know it's an old post, but since I got the same problem, following the same tutorial, I think I could reply and maybe it could help the next beginner to start with the STM8.. so you simply need to declare the assert_failed function in your main.c. just have a look in the STM8S Peripheral Library, look in any example at the end of a main.c file, you got :#ifdef USE_FULL_ASSERT
/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { } } #endif and it's also probably possible if you don't want to add this code to undefine USE_FULL_ASSERT, since it's here in an #ifdef. but I didn't look yet where in the library you can set that..... ffred2014-01-25 11:40 AM
Hi, I am new here and got the same problem, luckily, I didn't had to break my head and I found this post quickly.
Does anyone know how to load this code into the discovery board (step by step)? I tried using STVP but nothing is happening. Not sure if I have the right settings. I am really struggling with that. ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.