2011-11-16 2:27 AM
I configured the PC4 and PC7 ports both as inputs:
GPIO_Init(GPIOC, GPIO_Pin_7, GPIO_Mode_In_FL_No_IT); GPIO_Init(GPIOC, GPIO_Pin_4, GPIO_Mode_In_FL_No_IT); I would like to use these two pins with the ADC (channel 3 and 4 respectively) showing the voltage value on the on-board LCD. If I setup a program to do this with PC7 all behaves normally. If I do the same for PC4 when I apply a (constant) signal (say 0 V) the LCD goes mad and the program appears to reset. Checking with a scope PC4 is stuck to 3 V while PC7 is at 0 V, both with the same configuration written before. Could PC4 pin be somewhat broken or am I doing something wrong? EDIT Example: void main(void) { GPIO_Init(GPIOC, GPIO_Pin_4, GPIO_Mode_In_FL_No_IT);; //Green light on GPIO_Init( GPIOE, GPIO_Pin_7, GPIO_Mode_Out_PP_High_Fast); /* Set System Clock divider to 1 */ CLK->CKDIVR = 0x00; } This code just turn the on-board green led ON. When I try to apply 0 V to PC4 the led starts blinking... I think it is a hardware failureWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.