2009-07-15 9:45 AM
STVD 4.1.2 STM8 simulator error
2011-05-17 6:03 AM
Dear Sirs,
the attached project is a subset of my project. When I use the STVD to simulate a STM8S207C8, strange things happen near row 129 of main.asm It seems that the synhronization between the simulator and the STVD interface is lost, and this makes STVD useless. Regards, EtaPhi2011-05-17 6:03 AM
Dear Customers,
The assembler absolute list file main.lst is incorrect. Some instructions are not optimized in the list file while they are in the code. For example: LDW {CoRoutineSP+{Sicur_ID shl 1}},X is assembled in the list file as CF0006 while in the code it is assembled as BF06. As STVD uses the absolute list file to get debug information, it is lost. However there is a workaround: use #define instead of EQU. Just replace all EQUs by #defines in glob.inc. Regards, RJ2011-05-17 6:03 AM
Robert,
many thanks for your fast reply, as always... Regards, EtaPhi [ This message was edited by: EtaPhi on 16-07-2009 05:32 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.