Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Dear Sir/Madam,Using ST490ABDR IC as RS485in the Weather Monitoring project. The device is not working with multiple MODBUS slave. I observed signal level on the Oscilloscope, it is dropped at the time of query. Please find attached Schematic and wav...
Hi,I have two X-NUCLEO-GNSS1A1 expansion boards.I powered on the first board, and connected to UART port. I can read GPS messages from the board. GPS location is good. (I got GPRMC and GPGGA, GPGLL, etc.) I don't know what I did. Somehow NMEA messag...
Hello,I am working with STM32F4 discovery.I want to use EEPROM to write and read data. I have taken example code from https://github.com/PaxInstruments/STM32CubeF4/tree/master/Projects/STM32F4-Discovery/Applications/EEPROM/EEPROM_Emulation and it wor...
Would like to know do the below parts RoHS 2015/863 compliance?If yes, can provide the certificate ?ST Micro M74HCU04RM13TRST Micro M74HC109RM13TR
Hello,I am building a project which involves reading analog signals from 2 sources.I want to read ADC in interrupt mode. Please share some code or example or tutorial ?Mcu: STM8S103F3PIDE/Compiler: STVDLibrary: Standard Peripheral Library
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.