2007-04-18 10:57 PM
2007-04-18 6:27 AM
:-Y I'm frustrated trying to get the I2C to generate an interrupt when I set the STARTGenerate bit. I can use the I2C in polled mode talking to my slave device without any problems. But when I move to IRQ based communications the I2C never IRQ's! I have the following code as my main() and set a breakpoint in the STR71x_vectors.c I2C0_IRQHandler() and I never get there.
Before calling I2C_STARTGenerate, I2C0->CR has a value of 0x25 and the I2C0->SR1 has a value of 0x00. When I call I2C_STARTGenerate I2C0->CR stays the same and I2C0->SR1 has a value of 0x93. But I never get an IRQ. What am I missing? Here is my code: EIC_Init(); GPIO_Config( GPIO1, 0x6000, GPIO_AF_OD ); I2C_Init( I2C0 ); I2C_FCLKConfig( I2C0 ); I2C_OnOffConfig( I2C0, ENABLE ); I2C_AddressConfig ( I2C0, 0, I2C_Mode7 ); I2C_SpeedConfig( I2C0, 400000 ); I2C_AcknowledgeConfig( I2C0, ENABLE ); I2C_ITConfig( I2C0, ENABLE ); EIC_IRQChannelPriorityConfig( I2C0ITERR_IRQChannel, 2 ); EIC_IRQChannelConfig( I2C0ITERR_IRQChannel, ENABLE ); EIC_IRQChannelPriorityConfig( I2C0_IRQChannel, 7 ); EIC_IRQChannelConfig( I2C0_IRQChannel, ENABLE ); EIC_IRQConfig( ENABLE ); I2C_STARTGenerate( I2C0, ENABLE );2007-04-18 10:57 PM
Here is my code, and it does generate an interrupt:
Code:
/* Configure relevant port lines as Alternate Function, Open Drain */
IOPORT0_PC0 &= ~0x000C; IOPORT0_PC2 |= 0x000C; I2C1_OAR2 = 0x40; /* System frequency range: 16.67-26.67 MHz */ I2C1_CCR = 0x92; /* Bus clock = 397 kHz */ I2C1_CR = 1 << 5; /* Enable peripheral */ I2C1_CR = 1 << 5 | /* Enable peripheral */ 1 << 2 | /* Enable acknowledge */ 1; /* Enable interrupts */ EIC_SIR8_bit.SIPL = DAC_PRIORITY; /* Configure the channel 7 priority */ EIC_SIR16_bit.SIPL = DAC_PRIORITY; /* Configure the channel 15 priority */ EIC_IER0 |= (1<<8 | 1<<16); /* Enable interrupt on channels 7, 15 */ I2C1_CR_OFF |= 1 << 3; /* Set START bit */There are two interrupts associated with an I2C. Make sure you are looking at the right one. Also pay attention to this note from the manual: Note: To enable the I2C interface, write the I2Cn_CR register TWICE with PE=1 as the first write only activates the interface (only PE is set).I don't know if the library does this for you. It probably does, since you are reading I2C0_CR as 0x25, which is the correct value. Regards, - mikeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.