2003-04-10 1:04 AM
STPC Elite - SDRAM controller configuration problem
2003-04-09 9:23 PM
I use STPC Elite with WindBond SDRAM (w986432dh-7). I have a problem to configure the SDRAM Controller REGISTER 0 (MEM_ REG0):
In the MEM_REG0 there are 3 parameters that represent tRP, tRCD and tRC: tRP (Precharge to Row Active - called PRA in MEM_REG0) is represented by two bits (Bits 16-15) PRA. In my SDRAM datasheet, tRP has value of 20ns – what value should I set to PRA? tRCD (RACTIVE to Read/ Write - called RRW in MEM_REG0) is represented by three bits (Bits 10- . In my SDRAM datasheet, tRCD has value of 20ns – what value should I set to RRW? tRC (Refresh Cycle Timing - called RCT in MEM_REG0) is represented by four bits (Bits 3-0). In my SDRAM datasheet, tRC has value of 65ns – what value should I set to RCT? Thanks2003-04-10 1:04 AM
I suggest that you go the following URL to determine the value of the mem01 register;
http://www.stmcu.com/files/mcu/regset.htm#memoryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.