2003-04-09 5:08 PM
release of ICP pins after programmation
2003-04-08 3:47 PM
After programming a ST72264 via the ICP socket (EPB10 board), the firmware can't be run automatically, coz' the ICP pins are not released (I guess the reset pin is still pulled down...). I have to take out the socket or reconfigure the target (by choosing the same one for example).......Could it be corrected in the next release?
2003-04-09 1:56 AM
It's not so clear, what do you mean? You want to run your device on the EPB socket? It's not the purpose of the EPB.
If your device is on an application board, effectively to run it, you have to remove the ICC cable cause the reset line is maintained low.2003-04-09 5:08 PM
Of course my intention is not to run the firmware on the EPB!! The point is that the reset line should be released after the programmation via the ICP cable, like the softec kit, so that I don't need to diconnect & reconnect the socket.
B.Rgds FWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.