2023-09-08 4:08 AM
Hi Sir ,
This is kishor ,we are using stm8s207mb in our application, some board are working in debug mode only , when we come out from debug its not running . iam not able to understand the problem . is there any ide issue or hard ware issue . we noticed one point in working board Reset Pin maintaining 3.5v, in the problem board it is below 2.6v . but we are using same components in all boards ....
please help me these problem Thank you.......
2023-09-08 4:35 AM
Welcome @kishor, to the community!
There are a myriad of possible scenarios why the STM8 won't work for you without a debugger connected. Without more details on the environmental conditions (schematics, parameters, etc), probably nobody is able to help you.
For example, pin NRST on the STM8S207 is a bidirectional pin, as you can see from RM0016, section 8. You should therefore look at this pin with an oscilloscope and not just measure a DC voltage with a multimeter.
Furthermore, for proper work, cleanly created software is necessary - it is certainly not exactly the same as in the other, working boards, is it?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.