2021-07-02 1:24 AM
Hello, I need to make this stm8s105c6 to control an 3.0 V PMDC motor using timers and microcontroller's clock. Also, I need to use pwm and this driver: EV - VNH7040AY. Timers:
I am totaly new and idk how to declare / write complicated sequences. I created an prototype with arduino and L298N. It is possible to translate it to STVD? Any suggestions? Thanks for attention!
Source code Arduino:
// PWM PROTOTYPE - DC MOTOR CONTROL USING ARDUINO UNO AND L298N MOTOR DRIVER - BUSARU ROBERT - CRISTIAN
//Initializing pwm pin
int ena = 10; // pwm pin
int in1 = 2; // motor direction
int in2 = 4; // motor direction
//Initializing timers;
int tim1 = 3000; // acceleration time
int pwm1 = 255;
int tim2 = tim1 + 2000; // nominal power time
int pwm2 = 255;
int tim3 = tim2 + 3000; // deceleration time
unsigned long myTime; // clock
void setup() {
//Declaring pwm pin as output
pinMode(ena, OUTPUT);
pinMode(in1, OUTPUT);
pinMode(in2, OUTPUT);
//Declaring Serial Monitor to see timers and what happen there;
Serial.begin(9600);
}
void phase1() {
myTime = millis();
Serial.println(myTime);
}
void loop() {
myTime = millis();
Serial.println(myTime);
if (myTime <= tim1) { //TIM 1 -> accelerating time
// currencyTime = myTime;
for (int i = 0; i < pwm1; i++) {
analogWrite(ena, i);
}
Serial.print("Accelerare: ");
} else if (myTime > tim1 && myTime < tim2) { //TIM 2 -> nominal power time
// currencyTime = myTime;
analogWrite(ena, pwm2);
Serial.print("Nominal: ");
} else if (myTime >= tim3 && myTime <= tim3 + tim2 + tim1) { //TIM3 -> deceleration time
for (int i = pwm2; i >= 0; i--) {
analogWrite(ena, i);
if (i == 0 && myTime > tim1 + tim2 + tim3) {
analogWrite(ena, 0);
myTime = 0;
}
}
Serial.print("Decelerare: ");
}
digitalWrite(in1, HIGH);
digitalWrite(in2, LOW);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.