2019-05-18 12:45 AM
Hi
I am using stm8s103 controller and stlink programmer on Ubuntu.
I have configured the system with SDCC for STM8S controller.
I am getting following error while writing binary in flash.
Following is the error i am getting,
Determine FLASH area
Due to its file extension (or lack thereof), "blink.ihx" is considered as INTEL HEX format!
245 bytes at 0x8000... Tries exceededLooks like programmer is not able to flash...
any help will be appreciated.
2019-05-19 2:05 AM
You get this error message, usually, when the SWIM connection is not functional.
Please check your SWIM connection and that the MCU in powered and functional (Reset & SWIM pins!).
Do you use the standalone StlinkV2 programmer or some development board with integrated Stlink interface?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.