2021-07-15 2:58 AM
#include "stm8s.h"
#include "stdio.h"
#define Relay_1_Port (GPIOB)
#define Relay_1_Pin (GPIO_PIN_5)
#define Relay_1 '1'
#define LED_1_OFF_Port (GPIOC)
#define LED_1_OFF_Pin (GPIO_PIN_7)
#define Read_fun '0'
#define Write_fun '1'
#define HIGH '1'
#define LOW '0'
#define DEBUG_SERIAL_ECHO_BACK // fOR DEBUGGING
#define DEBUG_RECEIVED_FUNCTION_FROM_SERIAL
static void CLK_Config(void);
static void UART1_Config(void);
void Delay(uint32_t nCount);
char Serial_read_char(void);
void Serial_print_char (char value);
bool Serial_available();
void Serial_print_string (char string[]);
static char *cmd = "AURA-TC:" ;
static uint8_t cmd_cmpr = 0;
void main(void)
{
CLK_Config();
GPIO_Init(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin, GPIO_MODE_OUT_PP_LOW_FAST);
GPIO_Init(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin, GPIO_MODE_OUT_PP_LOW_FAST);
UART1_Config();
Delay(100000);
while (1)
{
if (Serial_available() > 0)
{
cmd_cmpr = 0; // RESET
char data[20] = {0};
for (int i = 0; i < 8; i++)
{
data[i] = Serial_read_char();
#ifdef DEBUG_SERIAL_ECHO_BACK
Serial_print_char(data[i]);
#endif
if (data[i] == *(cmd + i))
{
cmd_cmpr = 1;
}
else
{
cmd_cmpr = 0;
break;
}
}
char Read_write_fun = Serial_read_char();
char Relay_num = Serial_read_char();
char Write_High_Low = Serial_read_char();
#ifdef DEBUG_RECEIVED_FUNCTION_FROM_SERIAL
Serial_print_string("\n----- Received Command code --------\n");
Serial_print_char(Read_write_fun);
Serial_print_char(Relay_num);
Serial_print_char(Write_High_Low);
#endif
if (cmd_cmpr)
{
if (Read_write_fun == Write_fun)
{
if (Relay_num == Relay_1)
{
if (Write_High_Low == HIGH)
{
GPIO_WriteLow(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin);
GPIO_WriteHigh(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin);
}
if (Write_High_Low == LOW)
{
GPIO_WriteLow(Relay_1_Port, (GPIO_Pin_TypeDef)Relay_1_Pin);
GPIO_WriteHigh(LED_1_OFF_Port, (GPIO_Pin_TypeDef)LED_1_OFF_Pin);
}
}
}
}
}
// ================= This is Problem ====================
// Delay(10000); if putting this the serial receiving not working properly
}
}
void Serial_print_string (char string[])
{
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET); //wait for sending
char i = 0;
while (string[i] != 0x00)
{
UART1_SendData8(string[i]);
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
i++;
}
}
char Serial_read_char(void)
{
int read_count_var = 0;
while (UART1_GetFlagStatus(UART1_FLAG_RXNE) == 0)
{
read_count_var++;
Delay(1);
if (read_count_var >= 100) {
break;
}
}
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
UART1_ClearFlag(UART1_FLAG_RXNE);
return (UART1_ReceiveData8());
}
void Serial_print_char (char value)
{
UART1_SendData8(value);
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET); //wait for sending
}
bool Serial_available()
{
if (UART1_GetFlagStatus(UART1_FLAG_RXNE) == 1)
return TRUE;
else
return FALSE;
}
static void CLK_Config(void)
{
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
}
static void UART1_Config(void)
{
UART1_Init((uint32_t)115200, UART1_WORDLENGTH_8D, UART1_STOPBITS_1, UART1_PARITY_NO,
UART1_SYNCMODE_CLOCK_DISABLE, UART1_MODE_TXRX_ENABLE);
UART1_Cmd(ENABLE);
}
void Delay(uint32_t nCount)
{
while (nCount != 0)
{
nCount--;
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line)
{
while (1)
{
}
}
#endif
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.