2017-09-01 9:10 PM
Hello.
I want to using uart1 with STM8S103K,
i do (already work):
1. write program to display 4 pieces of 7 segment.
2. define STM8S103 in STM8S.h
after add
stm8s_uart1.c and stm8s_uart1.h and build project, the compiler(Cosmic) tell error
'stm8s_uart1.c bad struct/union operand'
it's look like somethings not define to project.
Help please.
2017-10-23 5:27 AM
Well, compiler errors usually refer to 1 or more specific lines from a source file.
Without seeing those lines (and the declarations of the objects and function from those lines) people on the forum won't be able to tell you anything over what the compiler is already telling you.
Philipp
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.