2010-11-30 1:31 AM
hello all
Please find attached file source code and resources on my recent personal project.
Stm8s-Discovery is interfaced with astts75 chip (digital I²C temprature sensor) and a graphic serialdisplay of the manufacturer μOled 96-SG1 4DSystems.
The accuracy of the temperature sensor can beselected by softwarefrom 0.5 ° C, 0.25 ° C, 0125 ° Cto 0.0625 ° C.
The scale measuring ranges from -55 ° C to +125 ° C.
The main program just displays the temperature on μOled with 0.5°C of accuracy.
I hope to improve this project very soon.
You can find the datasheet of stts75 here:
http://www.st.com/internet/analog/product/169jsp
4DSystems μOled display and serial here:
http://www.4dsystems.com.au/prod.php?id=77
Regards
Romain.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2010-12-01 6:12 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.