Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unexpected error from ST Visual Develop

Hi there!I just want to open those workspace that I created before and find that all of them come with this error. I have not changed anything including path of libraries and workspac. Could someone point out how does this error come out and how to f...

MT.2 by Associate II
  • 1236 Views
  • 0 replies
  • 0 kudos

Compiler licence problem ?

Hi,i've installed STVD, download and install Cosmic Compiler for STM8 (free version with unlimited size). I've registered compiler and receive license file. I've forgot copy license file into lincence subfolder in cosmic installation folder. When i'v...

Resolved! PD Soft Reset doesn't work

Hello,I have developed an application which can dynamically detect source capabilities by reading the capabilities soon after a PD charger is plugged in. In order to renegotiate with the new PDO, I currently must issue a reset by writing to the RESET...

jefflongo by Associate III
  • 4540 Views
  • 8 replies
  • 0 kudos

Behavior of POWER_OK2 pins and GPIO pins STUSB4500

Here is my requirement for my USB-C powered system:I need 5 V @ >= 3 A.It doesn't really matter to me if the above is achieved from a USB PD contract in place, or if a non-PD USB-C Source is advertising 5 V @ 3A via a 10k pull-up.I don't want to use ...

MCapu.2 by Associate II
  • 2767 Views
  • 5 replies
  • 0 kudos

Not Detecting ST10F276 controller

HiActually I downloaded the ST10Flasher 2.4B and checked with ST10F276 Controllergetting the No acknowledge ErrorI have done P0L.4 to GND and P0L.5 to HIGH and did reset the controllerplease give me solution

EPunn.1 by Associate II
  • 1924 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.