2019-09-21 2:14 AM
Further to my previous message I have setup a new STVD workspace, included stm8s.h and just stm8s_adc1.c and .h, setup processor etc and get 150+ compiler errors on stm82_adc1.c just as if the header file was not specified but it is. So having reduced code to a minimum I still cannot see why these faults are being thrown.
Can anyone point me at the problem please?
I wonder if it might be better to abandon the SPL and just code what I need. What is the forum opinion on this as well?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.