2019-09-20 7:57 AM
My project uses the ADC on an STM8S and as it compiles using Cosmic the stm8s_adc1 module throws a huge number of compiler errors as follows:
Compiling stm8s_adc1.c...
cxstm8 +modsl0 +debug -pxp -no -pp -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\Hstm8" -clDebug\ -coDebug\ stm8s_adc1.c
#error cpstm8 stm8s_adc1.c:54(8+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:55(8+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:56(8+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:57(8+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:58(8+4) bad struct/union operand
#error cpstm8 stm8s_adc1.c:59(8+4) bad struct/union operand
...
#error cpstm8 stm8s_adc1.c:634(34+5) bad struct/union operand
#error cpstm8 stm8s_adc1.c:639(32+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:630(28+4) ADC1 undefined
#error cpstm8 stm8s_adc1.c:634(28+4) ADC1 undefined
#error cpstm8 stm8s_adc1.c:639(26+4) ADC1 undefined
#error cpstm8 stm8s_adc1.c:675(12+5) bad struct/union operand
#error cpstm8 stm8s_adc1.c:679(12+5) bad struct/union operand
#error cpstm8 stm8s_adc1.c:684(10+3) bad struct/union operand
#error cpstm8 stm8s_adc1.c:675(6+4) ADC1 undefined
#error cpstm8 stm8s_adc1.c:679(6+4) ADC1 undefined
#error cpstm8 stm8s_adc1.c:684(4+4) ADC1 undefined
stm8s_adc1.c:
The command: "cxstm8 +modsl0 +debug -pxp -no -pp -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\Hstm8" -clDebug\ -coDebug\ stm8s_adc1.c" has failed, the returned value is: 1
exit code=1.
My code simply calls ADC1_DeInit() and then init code.
Any ideas what I am doing wrong or what I need to do please?
Cheers, Bruce
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.