2018-06-03 11:05 PM
Hello
I'm use STM8L151G6
I'm trying use block programming as below://Unlock EEPROM memory
FLASH_Unlock(FLASH_MemType_Data);
while (FLASH_GetFlagStatus(FLASH_FLAG_DUL) == RESET);
FLASH_ProgramBlock(0, FLASH_MemType_Data, FLASH_ProgramMode_Standard, buffer);
while(FLASH_GetFlagStatus(FLASH_FLAG_HVOFF) == RESET);�?�?�?�?�?�?
But cpu always stops inside FLASH_ProgramBlock function, between instructions :
/* Standard programming mode */
FLASH->CR2 |= FLASH_CR2_PRG;�?�?
and
/* Copy data bytes from RAM to FLASH memory */
for (Count = 0; Count < FLASH_BLOCK_SIZE; Count++)
{
#if defined (STM8L15X_MD) || defined (STM8L15X_MDP)
*((PointerAttr uint8_t*) (uint16_t)startaddress + Count) = ((uint8_t)(Buffer[Count]));
#elif defined (STM8L15X_HD)
*((PointerAttr uint8_t*) (uint32_t)startaddress + Count) = ((uint8_t)(Buffer[Count]));
#endif
}�?�?�?�?�?�?�?�?�?
Therefore, I ask for help.
#stm8l #eepromWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.