Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L9362: Clamping energy specification

Hello,I'm using smart low-side driver L9362 and I'm confused about clamping energy information presented on datasheet:-in absolute maximum rating is declared an energy clamping limit of 50mJ with 2ms pulse width, 10ohm, 16mH-in figure 8 is declared a...

AD Am.1 by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos

Resolved! How to calculate TVS diode SMA6J33CA for ambient 105 °C

Hello ST team,I have trouble to calculate Tj and Rd for ambient 105 °C. What was my stepsApplications conditions for protection:Vin_max = 30 VVin_absolute = 58 VTamb_max = 105 °CMax surge current for 8/20 μs pulse wave:Isurge_max = 1 kV / 42 Ohm = 24...

0693W00000WHqzwQAD.png 0693W00000WHqytQAD.png
Reha by Associate
  • 4224 Views
  • 2 replies
  • 1 kudos

Resolved! Issue with UART1 in STM8S001J3

Hello, I'm having some problems with UART1 in STM8S001J3. I'm using the simple code below (the compilation is ok), but when I try to programming the MCU in STVP, a error happen and the MCU doesn't work anymore, even though I try to programming with a...

0693W00000NpnGCQAZ.png
VScar.1 by Associate II
  • 4397 Views
  • 7 replies
  • 0 kudos

I try to disable the SWIM interface in a STM8AL3168 derivative but it does not seem to work (see details). What am I doing or thinking wrong?

I try to disable the SWIM interface in a STM8AL3168 derivative, by setting the SWD bit of the global configuration register (CFG_GCR) = 1 in main().typedef struct CFG_struct{ __IO uint8_t GCR; /*!< Global Configuration register */}CFG_TypeDef;#define...

KGirs.1 by Associate
  • 2244 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.